How to display "Properties" in [New] Dialog? Properties are not displayed as shown below.
Steps to reproduce the problem-
Run in TCIN environment.
(1) Select [File]-[New]-[Item]
(2) Confirm Dialog. Properties is not displayed
Similarly, "Properties" is not displayed on NX 1980 in the TCIN environment.
However, "Properties" is displayed on NX 10.0.3.5 in the TCIN environment.
Also, the "Properties" is displayed on NX 1953 in a Native environment.
Solution
Currently, this is working as a design. All these properties are now added to the Column Configuration in the NX File > New Dialog. Refer to the below snapshot.
Notes and References
10120996
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: NXMANAGER Version: V1953 Function: FILE_NEW